5/23/2011 8:50 AM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
"ASO Error" can be caused by mixing different version of WinCC & SQL (+service packs + updates) like you said that your server is winCC v7 SP2 & clients are v7 SP1. |
Last edited by: SteBo at: 5/23/2011 8:52 AMWInCC v7 & V7 SP1 use both SQL Server 2005 SP2 WInCC V7 SP2 uses SQL Server 2005 SP3 B r g d s , |
|
This contribution was helpful to1 thankful Users |
5/23/2011 9:57 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Is raw data communication via "Named Connections" supported in WinCC V7.0 SP2 and WinCC/powerrate? Perhaps How are called and interconnected the SIMATIC Powerrate library blocks in STEP 7 and WinCC? How do you use SIMATIC powerrate library blocks in PCS 7? Best regards, Hristo Mihalev |
Follow us on