(0)| 12/29/2006 10:27 PM | |
|
Posts: 42 Rating:
|
[:blush:] I hope someone can HELP me with usage of DP/DP couplers.I have one Master on the left marked as Master1 (profibus network 1) and I have five masters on the right, marked as Master2, Master3.....Master6. (profibus network 2) and betwen them a DP/DP coupler.I wont to send data from Master2 to Master1, Master3 to Master1, Master4 to Master1.....Master6 to Master1. I wonder is this posible if I use only one DP/DP coupler or I must use coupler for evry pair of Masters (that means 5 couplers)...... All Masters are CPU 315-2DP AttachmentProfibus couplers.zip (825 Downloads) |
Follow us on