9/19/2011 7:44 PM | |
Joined: 5/4/2009 Last visit: 4/30/2024 Posts: 914 Rating: (40) |
Dear friends, Here is my ordeal now, I have a costumer dealing with the CPU314IFM, but during compilation it showed me that there isconflictregarding data types in FC32 and it refused to be downloaded (please refer to the attached files it contains the compilation report and the project itself). Please advice what to do... Thank you in advance. Tomy.
Attachmentsoft_ware.zip (31 Downloads) |
Aim Higher |
|
9/20/2011 11:30 AM | |
Joined: 5/4/2009 Last visit: 4/30/2024 Posts: 914 Rating: (40) |
Dear yy1, I have referred to help files and I did create a new DB180 for FB41 instead of DB80, then all error was solved except that for FC32, then I saw your kind reply and I did the first solution suggestion then it seems that the problem are solved but still some warnings. (Pleasse refer to attached). Warm regards. Tomy.
AttachmentModified_Project.zip (26 Downloads) |
Aim Higher |
|
This contribution was helpful to1 thankful Users |
Follow us on