10/13/2011 8:40 AM | |
Posts: 327 Rating: (28) |
Greetings By mobile device you mean mobile phones? If you wan't to send just alerts and few numbers, you can use GSM modem to send SMS. You have a (relatively) cheap existing solution here:https://support.automation.siemens.com/WW/llisapi.dll/40616248?func=ll&objId=40616248&objAction=csView&nodeid4=20229805&lang=en&siteid=cseus&aktprim=4&extranet=standard&viewreg=WW&load=content Another option, if you have smartphone, is using applications for remote desktop. E.g. we use TeamViewer and we are able to access our HMI from any newer smartphone or any PC with connection to Internet. Best regards
|
This contribution was helpful to1 thankful Users |
10/18/2011 7:24 AM | |
Posts: 327 Rating: (28) |
Greetings Yes, you get Basic verison of WinCC with Step7 Basic, but this edition is only for Basic Panels and not PCs (https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=49740133&objAction=csOpen&nodeid0=47069298&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW) You should go for WinCC v11 Advanced edition, which allows you making applications for PC. Or, you can use WinCC flexible 2008 SP2, which is pretty much the same as Advanced, only it is not integrated in new TIA Portal. Best regards
|
This contribution was helpful to1 thankful Users |
10/25/2011 10:08 AM | |
Posts: 327 Rating: (28) |
Greetings You have said you will measure pH, conductivity, etc. These are all analog values, so you need analog sensors and analog input modules... For the voltage measurement, there is an analog input module for signal -10...+10V, but this is not intended for general measuring of voltage. You can find technical descriptions of modules in here:https://support.automation.siemens.com/WW/llisapi.dll/36932465?func=ll&objId=36932465&objAction=csView&ClusterID=41737332&nodeid0=34612486&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=content&subtype=133300 Best regards
|
Follow us on