12/2/2011 10:52 AM | |
Posts: 7 Rating: (0) |
Hello, Sometimes when I want to enter the custom screen I get this error : "error QW_LoadOverlay: aggr_man.dll". What does it mean? Thank you. |
1/13/2012 2:21 PM | |
Posts: 7 Rating: (0) |
My problem is still unresolved. While the machine is working and the operator uses the custom screen trying to introduce parameters , after a while (cannot verify when or at which screen) the cnc control blocks, so we have the restart the machine. I don't know where is my problem so I attached an xml written for my custom screen. The remaining xml are almost the same. Please , help! Thank you.
Attachmentt1.zip (57 Downloads) |
1/16/2012 6:00 PM | |
Posts: 54 Rating: (8) |
Hi, I checked the file enclosed and tried to understand that script snipped. You will find a version where I reduced the instructions in the softkey tags. It is not necessary to control the pressed or not-pressed state of a softkey if you want to navigate to a other menu. It can be used, if you do not leave the current menu. The softkey tag softkey_back shows the face automatically. It should be used to return to a upper menu level. The control attribute type="real" is not necessary because the refvar attribute defines the format. It has a meaning if you want show a PLC variable as floating point value. All names of forms and menus should be unique in one project. Please check your softkey definitions. I guess that the problems come from the softkey programming. Best regards drill_easy Attachmentt1_1.zip (53 Downloads) |
Follow us on