2/1/2012 6:09 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Updates for STEP 7 V11 SP2 and WinCC V11 SP2 Can you post a screen shot of that message? best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
2/2/2012 10:30 AM | |
Joined: 10/7/2011 Last visit: 3/6/2024 Posts: 28 Rating: (2) |
I have installed Updates for STEP 7 V11 SP2 and WinCC V11 SP2 but tia portal need other udate see attachment |
2/2/2012 11:34 AM | |
Joined: 8/31/2010 Last visit: 10/15/2024 Posts: 1522 Rating: (228) |
Hello Bizz, It doesn't seem like that. See the Timeline of softwares released in ascending order as mentioned below. TIA Portalv11 TIA Portal v11 Update 1 TIA Portal v11 Update 2 TIA Portal v11 SP1 TIA Portal v11 SP1 Update 1 TIA Portal v11 SP2 TIA Portal v11 SP2 Update 1 The last one "TIA Portal v11 SP2 Update 1" has all the above mentioned. If you have the TIA Portal v11 SP2 Update 1 (both STEP 7 v11 SP2 Upd 1 and WinCC v11 SP2 Upd1) then you don't need to worry about your screenshot. Also can you pls post screenshot in english? |
Like it? Rate it! |
|
Follow us on