2/9/2012 3:27 PM | |
Joined: 12/13/2011 Last visit: 10/1/2024 Posts: 146 Rating:
|
I thinkwhat'slostcontrol of theencoderyou couldreview theearth if there isgoodgroundconnectionfails andstops theservo |
2/15/2012 5:08 PM | |
Joined: 8/31/2005 Last visit: 8/8/2025 Posts: 2198 Rating:
|
Ok, you habe a SINAMICS S110 and a SIMATIC connected with PROFINET. If you do not use DRIVE ES, you will have to configurate the communication twice: on time in STEP 7 (HW Config) and the 2nd time in STARTER (the SINAMICS parametration tool). Make shure the to define exact the same, see attachment. If you use DRIVE ES you add the drive in HW Config and configurate it in STARTER. With DRIVE ES you will find a button "Transfer to HW Config". This will copy the configuration into HW Config. So you only have to add the data one time. I think, in STEP 7 (PLC, Edit Ethernet node...) you must assign the IP to the drive, bevor you can communicate with it. The drive must be connected (to the PG/PC), you must search it (Browse...), select it and give a PN- device name (Assign Name) AttachmentS110.zip (402 Downloads) |
Last edited by: miami at: 2/15/2012 5:10 PM |
|
Follow us on