2/18/2007 6:22 PM | |
Posts: 2 Rating:
|
How is the connection of wire? |
2/19/2007 8:04 AM | |
Posts: 2930 Rating:
|
Hi all, since a view days the Micro/WIN SP5 is avaliable. If you have installed the Instruction Library for STEP 7-MicroWIN and you install the SP5 then you get the official new Libraries. The new libraries are: 1. USS protocoll for Port 0 and 1 2. ModbusRTU Master for Port 0 and 1 Here you can download the MicroWIN SP5: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=de&siteid=csius&aktprim=0&extranet=standard&objid=24676421&DataKey=24676421&treeLang=de If the link does not work, then goto the Siemens Support pages and look for the ID 24676421 I hope this helps Regards Helmut |
Follow us on