3/11/2012 6:04 PM | |
Joined: 8/31/2010 Last visit: 5/28/2024 Posts: 1514 Rating: (223) |
Hello Ahmed Mandor, Check this FAQ on SINAMICS / MICROMASTER 4: Use of STARTER and STEP7 V11 together with Siemens frequency converters. The GSD file for MM440 can be found here - MICROMASTER 4: Amended PROFIBUS GSD files (inc. MICROMASTER 411, 420, 430 and 440) Additional you can refer this Application example, here instead of SINAMICS you are using MICROMASTER - Connecting a SINAMICS drive to an S7-1200 CPU in TIA Portal (via GSD file) |
Like it? Rate it! |
|
This contribution was helpful to2 thankful Users |
Follow us on