3/18/2010 10:39 AM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
Hi, I try to install WINAC RTX F 2009 on some PC (notebook or laptop), but when I try the evaluation tool to control the HW I recive the same answer "...the IRQ8 is not assigned to RTC" , but if you control the file at pag.4 is not true: the IRQ8 is assisgned. And also if I control from Device Manager teh IRQ8 IS ASSIGNED TO RTC. Normally We use RTX F on Siemens PC without problems, but in our laboratory we've other PC and we thought to use to them only for testing. Please can you helm me? Thanks, Diego Attachmenterrore.pdf (345 Downloads) |
3/19/2010 1:48 PM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
No idea ??? |
3/26/2010 11:16 AM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
...thank you...in english works. Ciao, Diego |
3/28/2012 3:21 PM | |
Joined: 8/24/2006 Last visit: 5/31/2024 Posts: 148 Rating: (9) |
Hi, what I've done it's to format ed install windows in english...I think there's a FAQ... |
Follow us on