4/23/2012 4:39 PM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191) |
Hello, one question, do you use PCS 7 or WinCC or nothing of both? Regards |
SIMATIC PCS 7 - Overview |
|
4/23/2012 5:28 PM | |
Posts: 13 Rating: (0) |
I use Simatic Manager Step 7, and also WinCC. But mostly Step 7. |
4/24/2012 9:28 AM | |
Posts: 272 Rating: (4) |
You can use the functionality of Web Navigator, where remote monitoring of data is possible. I think this request should be transferred from PCS 7. |
4/24/2012 9:31 AM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191) |
Hello, if you want to see some data, the you have to use WinCC. CFC Online and CFC Trend which are in the SIMATIC Manager areonly for testing of the engineering. Regards |
SIMATIC PCS 7 - Overview |
|
4/24/2012 9:54 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Adriann22, Have a look on the Application Example With Code. Documenting Operations Using WinCC WebNavigator But to Used this in your Project You need a License..... & as I know the Server with 3 Client will Cost to High for your Project. You can see the Functionality what you canused have a look on the Siemens Demo WinCC/WebNavigator and WinCC/DataMonitor demo access |
Ammy |
|
4/27/2012 9:37 AM | |
Posts: 13 Rating: (0) |
It's a wonderful idea and thank you for it, but unfortunetly, I can't afford to buy the license. Any other ideas, preferably that are free? :) |
4/27/2012 10:27 AM | |
Posts: 1064 Rating: (72) |
Try reading this link it might help you |
Follow us on