5/17/2012 4:07 PM | |
Posts: 150 Rating: (17) |
Dear all, What are the required OBs so that the cpu does not stop when a Profibus-DP slave fails. Regards |
5/17/2012 4:27 PM | |
Joined: 8/31/2010 Last visit: 5/20/2024 Posts: 1512 Rating: (223) |
Hello Nikzitronik, Check this FAQ under S7-1200 categories - Which organization blocks can you use in STEP 7 V11? |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
5/18/2012 1:41 PM | |
Posts: 150 Rating: (17) |
Firmware version is 2.2 and TIA portal V11. Regards |
Follow us on