6/18/2012 5:22 PM | |
Posts: 6 Rating: (0) |
Hello Can I use 1FT servo motor to run the spindle in a lathe? What parameters are to be set? which drive to use? FDD or MSD itself? regards sriraman |
6/19/2012 3:14 PM | |
Posts: 6 Rating: (0) |
Hello It is 840C with simodrive 611D drives. regards |
6/20/2012 8:47 AM | |
Posts: 2964 Rating: (479)
|
Hello.... If it is with 611A Control you can use the motor 1FT5 series.... Regards, Prakash |
Follow us on