4/3/2007 9:02 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, You program the CPU via the EM277 even whenb it is connected to Profibus. See also page 430 of the attachment. The attachment is a part of the S7-200 system manual, which can be downloaded at this link. AttachmentEM277 pages from S7200N_e-2.pdf (338 Downloads) |
Smurf |
|
Follow us on