6/29/2012 5:28 AM | |
Joined: 5/28/2008 Last visit: 6/8/2024 Posts: 4509 Rating: (837)
|
Hello, Yes the active bus unit cover part number is6ES7195-1JA00-0XA0. Normally we may use it if you have one bus module (for two 40 mm wide module) and only one 40mm module is available. I said "may" because it is not necessarily to use these covers. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on