7/1/2012 1:29 PM | |
Posts: 378 Rating: (73) |
Dear Zazu , Congrats for your success !!! and Thank you for thanking experts !!! Some of the members (including me) runs away after they got solution from this forum. I think it is good practice for the development of this forum to let know the result of the solution forwarded by forum members and experts. Thanks again |
7/1/2012 2:09 PM | |
Joined: 3/4/2011 Last visit: 11/1/2022 Posts: 78 Rating: (4) |
OK I've decide to upload the program and see if any of our experts can suggest ways to improve it. Just a couple of notes. The four function keys are used to set the preset meterage and I5 is the count input. I7 must be made for a reel change and reset to take place and I1 starts the winder which has to be on for the counter to function. I5 is set as frequency and maximum is 4100 which equates to 123 M/min. Enjoy.
AttachmentReifCounter80.zip (284 Downloads) |
Follow us on