7/1/2012 8:50 AM | |
Posts: 14 Rating: (0) |
Need Of GSD file for Siemens Simatic S7 6ES7-374-2XH01-0AA0 I/O Module . |
7/1/2012 9:41 AM | |
Joined: 10/7/2005 Last visit: 6/8/2024 Posts: 3008 Rating: (1051)
|
Hello msarapong the 6ES7374-2XH01-0AA0 is a Simulator module and you will NOT find a GSD file it as it isnot a Profibus DP Slave by itself, but simply a Signal module for an S7-300 and/or ET200M Profibus DP Slave station. Have a look at the Hardware update for 6ES7374-2XH01-0AA0 simulator module thread to find out how to configure and use it, should that be the information you are actually after. I hope this helps P.S: It would be greatly appreciated if you only post a question once in the future (posting the same question three times in three different conferences does not increase your chances of a receiving a useful answer). |
Last edited by: fritz at: 7/1/2012 9:42 AMtypos Cheers |
|
7/1/2012 4:22 PM | |
Joined: 5/28/2008 Last visit: 6/9/2024 Posts: 4509 Rating: (837) |
Hello, Siemens Simatic Module6ES7374-2XH01-0AA0is digital input, output or Input/Output simulator. It means that you can use this module in one of the following three configurations:
There is no gsd file for this module.
For any selection, do not forget to adjust the rotary switch to match the configuration in your HW config. Hope this helps.
|
Ayman Elotaify |
|
Follow us on