4/9/2007 10:24 AM | |
Posts: 8 Rating: (0) |
Hi, I have a big problem with a WinCC Flexible RT 2005 SP1 HF7. I have my laptop coneccted via MPI Card CP5512 to a S7300 CPU. I start mi application and while RT is runing the data get "stoped", "fridged" during sometimes 10-20sec and then gets back and doit again every 5-10min. I think the problem is the new laptop i have bougth. Is a DELL LATITUDE D820 with XP Prof SP2, with Duo Core. Here is the link for especifications: http://www1.euro.dell.com/content/products/productdetails.aspx/latit_d820?c=es&cs=esbsdt1&l=es&s=bsd&~section=specs#tabtop Because I have tested with 3 D820 and always goes quiet bad. But if i test with two of our not new laptop DELL LATITUDE D810 (which is not Duo Core!!!) its works perfect!!! DELL support tell me this two laptop models are completily diferent! Do you have some idea??? Thanks |
Last edited by: JaviM at: 09.04.2007 10:28 |
|
Follow us on