7/19/2012 11:27 AM | |
Joined: 7/2/2012 Last visit: 2/13/2024 Posts: 31 Rating: (0) |
we found a solution to the problem : we deactivate the handwheel in the DB200 of the S5 SPS -> DB200 word 80 : activation of the handwheel 'UN' and we deactivate it with putting 'UB' -> the S5 is running =>in the DB200, we found also that theadress of the hadwheel = 15 -> correspond to the error message 43 6F00 0400 0300 1500 0100 We tried to change the handwheel, the hadwheel interface card, the bus cable, but it doesn't work! So we don't have a handwheel anymore on the machine ... in attachement the "Doc on CD 840C" pdf file of the diagnostic PLC i hope this could be helpfullfor someone bye Attachment840c_da.pdf (217 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on