5/7/2012 4:59 PM | |
Joined: 6/25/2009 Last visit: 4/24/2024 Posts: 37 Rating: (5) |
Hello I'm still battling with F30011. I trended DC link voltage and current at the moment of fault and during normal operation. Can someone have a look at attachment and say if this is normal behaviour of the dc link voltage (supply voltage 525V)? Regards AttachmentPS-PMP-09 - Power unit Line phase failure in main circuit at the moment of F30011.JPG (340 Downloads) |
7/19/2012 7:51 PM | |
Joined: 6/4/2008 Last visit: 5/1/2024 Posts: 1484 Rating: (322) |
Hi, just a quick question, what is the firmware version on the CU320-2? Regards, Graeme
|
7/23/2012 5:10 PM | |
Joined: 6/4/2008 Last visit: 5/1/2024 Posts: 1484 Rating: (322) |
Hi, the rumour is there will be a firmware hotfix for this issue. Regards, Graeme
|
Follow us on