12/23/2011 5:39 PM | |
Joined: 10/18/2011 Last visit: 5/8/2024 Posts: 40 Rating: (0) |
when I connect cp341, pc, and speed measuring device together, I find the following: 1. PC send command, PC can receive correct reply. And CP341(FB7) receive the correct reply, too. 2. CP341 send command, PC received reply with the first character messed up. CP341(FB7)doesn't receive anything. shown in the attached. There is a collision during CP341 sending and receiving? Attachmentsend.zip (186 Downloads) |
Follow us on