9/26/2012 12:22 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello @Nick, Yes, it should be possible to monitor blocks in PLC. About your panel, perhaps the following link might help: What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC via the Internet (WAN)? Best regards, Wizard |
Last edited by: Wizard at: 9/26/2012 12:25 PM |
|
9/26/2012 4:44 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Nick, Perhaps this link might help: how do you use WinCC flexible to transfer a project to an operator panel via S7 routing? Best regards, Wizard |
9/27/2012 10:32 AM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Hi Wizard, I'm using MP 277 "8 Touch panels. Version 1.1.3.0, 2008 SP2 Thanks in advance!
|
9/27/2012 11:22 AM | |
Posts: 3037 Rating: (192)
|
Hello @Nick, You can use S7- Ethernet Routing with MP277 and WinCC flexible 2008 SP2. You can see more information about Routing in the following link. How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? Tweety |
9/27/2012 12:50 PM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Hi Tweety, If I open the document under mentioned, in the example they use a "WinCC flexible ES" in Netpro this option is not available in my project. I have used the PG/PC but this isn't working. " More information in manualMore information on the topic of "Project transfer via S7 Routing" is available in the WinCC flexible manual in Entry ID:18796010. " Thanks in advance!
|
9/28/2012 11:24 AM | |
Posts: 3037 Rating: (192)
|
Hello @Nick, What you mean with "they use a "WinCC flexible ES" in Netpro this option is not available in my project." Do you mean you can not see your MP277 station in Netpro? Can you post a screenshot about your Netpro configuration? A routing connection is only possible with integrated projects. Do you use an integrated project? Do you check if all modules using the function S7 routing? What are the requirements for using the S7 routing function and which modules can you implement? Tweety |
Follow us on