10/5/2012 1:05 PM | |
Posts: 510 Rating: (117) |
You didn't say when you wanted to change the time. TIA Portal can set the PLC time to the time of the PC. Here are a couple of links that might cover what you need. Here is a link to an FAQ on the time functions you can use to input the time: http://support.automation.siemens.com/WW/view/en/43566349?Datakey=47071380 Here is a link on synchronizing time between the 1200 and a Basic Panel http://support.automation.siemens.com/WW/view/en/39182145 Good Luck billwest |
This contribution was helpful to1 thankful Users |
Follow us on