11/9/2012 8:03 AM | |
Posts: 55 Rating:
|
I have MasterDrive with CBP2 (6SE7090-0xx84-0FF5) card whitch will be connected to PLC through Y-link. I need to read amps, power, temperature, operating hrs and status of DI I was planing to use SFC58/SFC59 to read these values acyclicly. But in a Y-link manual I see this: Which devices can be operated behind the Y Link? Slaves at the lower-level DP master system cannot be operated in DPV1 mode unless they have been integrated and configured with GSD rev. ≥ 5. The GSD must contain the following entries: ● Prm_Block_Structure_supp=1 ● PrmCmd_supp=1 ● Slave_Redundancy_supp=1 STEP 7 checks these entries during configuration. If these entries are not found, the slave is then operated in DPV0 mode. GSD file found at http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=48169112&caller=view of course doesn't contain these entries. Does it mean that CBP2 doesn't support DPV1 when connected behind Y-link or maybe there is newer GSD that enables DPV1 support for CBP2? |
Follow us on