1/14/2013 6:40 AM | |
Posts: 12 Rating: (0) |
Hi All, May i have a question about the sample program below? /tf/WW/en/Posts/57715 I have download the program and it work fine for the frist time, and i able to download the logging result via webserver. problem is , when i power OFF and ON the PLC, then i follow the same sequence to start the data logging, i found that, the block is not allow to create a data log file, and i was not able to log the data anymore, but then, it will work only when i go in to webserver and delete the perious log data. so can you please advice on this issue ? In the other hand, can you also please advice how the "Data Log Open" ; "Data Log Close" ; "Data Log New File" work on your program ? Thanks & Regards |
1/31/2013 2:06 PM | |
Posts: 267 Rating: (22) |
Hello, I don't know the program you mentioned, but when you try to create a data log csv that already exists, the block "DataLogCreate" willreturn an error. In the following program there is a sequencer which reacts to such an error: http://support.automation.siemens.com/WW/view/en/64396156 |
This contribution was helpful to1 thankful Users |
Follow us on