3/13/2013 10:41 AM | |
Posts: 1530 Rating: (59)
|
Hallo T.D.J, if I take a look at your dcf-files, I see that Prefix2 is missing in the one, which doesn't work. Did you already take a look at this: No variables displayed although you have a connection I think this could be solution to your problem, if not please let me know. Best regards Bizur |
3/14/2013 10:40 AM | |
Posts: 1530 Rating: (59)
|
Hello T.D.J, dcf-file is a system file. Normally user hasn't to do something with it or in it. If it doesn't work correct user may delete it and it will be created new (compare FAQ). Yes, I know in one of your first posts, you tried this and it didn't work. But at the moment I can only tell you something about the normal way it should work. But I don't think, that mapping your project (via Simatic Manager) will change something in dcf-file. I think this are two different things. Did you already check your diagnose files, when it wasn't working? Do you remember at any difference between situation when system was working fine after mapping and new one? Did you add/remove some equipment? Best regards Bizur |
3/14/2013 1:34 PM | |
Joined: 12/30/2009 Last visit: 11/30/2023 Posts: 18 Rating: (0) |
Yes, TDC Transfer |
Follow us on