(1)| 3/29/2007 7:37 PM | |
|
Posts: 3 Rating:
|
Attached is a Step 5 program. Part of that program controls 3 temperature zones on a machine, with thermocouple inputs and IP-262 closed loop control module. I am familiar with Step 5 but not so much with IP-262. Could someone take a few minutes to look at this program to define what DBs are used for the IP-262, and to give me some direction. I have the IP-262 manual but can't identify these for certain. I am adding 4 additional temperature zones to the machine....so I will need to "duplicate" some data areas and code.
Sorry...I don't have any symbols. Many Thanks!!!! Attachment3zhmacst.zip (557 Downloads) |
| 4/4/2007 3:38 PM | |
|
Posts: 3 Rating:
|
Thanks...but what is the purpose of FB62 and where is the information telling which slot the module is in? DW? in DB? ? Thanks again! |
| 6/7/2007 1:37 AM | |
|
Posts: 9 Rating:
|
Hi:: |
Follow us on