4/9/2013 7:42 AM | |
Joined: 4/19/2008 Last visit: 5/21/2024 Posts: 1525 Rating: (159) |
Hello Priyanka, I am not sure that you can able to make the Online trend with WinCC option because I have never come across it, SIMATIC Process Control System PCS 7 OS Process Control (V8.0 SP1) Have a look on the Chapter 7.1 in the Above manual. for all the information related to Trend. Also you will find the other topic related to Key set Button available via in OS Configuration on Chapter 4.8 |
Ammy |
|
4/9/2013 12:00 PM | |
Posts: 1530 Rating: (59)
|
Hello Priyanka V, Advanced Process Control is integrated in PCS7. In WinCC you use Basic Process Control via OS Project Editor. Best regards Bizur |
Follow us on