7/2/2013 8:18 PM | |
Posts: 25 Rating:
|
which OB must we use in S7-1200 "The idea is to add an integrated value from a scaled analogue signal, to a register every 100ms.At 60m³/h, the register should count up to 1 every minute, but it counts erratically. Never the same value, but always a lot more (10-20)"This works in a 300 using OB35 at 100ms. Any way to rectify this? Please see attached. AttachmentDoc1 PIC.pdf1.pdf (506 Downloads) |
Last edited by: O_Moderator at: 7/4/2013 2:13 PMfile reattached |
|
7/3/2013 9:22 AM | |
Posts: 25 Rating:
|
THANKS...... |
This contribution was helpful to
2 thankful Users |
Follow us on