7/12/2013 12:20 PM | |
Joined: 7/13/2009 Last visit: 10/7/2024 Posts: 137 Rating: (5) |
Hello Majeed, Have you checked theFAQ?
|
Thanks and Regards |
|
7/12/2013 12:23 PM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
Dear Majeed Ahmed, it could help if you would attach printscreens as a zip-file to your question. In that case, members can see what you're really talking about (for example, buildup of your screen and picture window) and if you're lucky, you'll get working code examples too. |
B r g d s , |
|
7/12/2013 2:07 PM | |
Posts: 55 Rating: (1) |
Thanks for the reply, Attachmentwincc_PassingPar.zip (189 Downloads) |
7/12/2013 2:31 PM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
Thanks for the extra info. Imo, if your single popup is well-defined. changing tag prefix should do the trick. Sometimes it's handy to use specific names for your objects, as you have the objectname automatic in your c-script too: a small example: // WINCC:TAGNAME_SECTION_START // WINCC:PICNAME_SECTION_START #define PicNameInAction "Testing.PDL" // WINCC:PICNAME_SECTION_END char cTagPrefix[30];sprintf(cTagPrefix, "%s.", lpszObjectName); SetTagPrefix(PicNameInAction,"Picture Window1",cTagPrefix); SetPictureName(PicNameInAction,"Picture Window1",lpszPictureName); .... combined with one of those below SetVisible(PicNameInAction,"Picture Window1",FALSE); |
B r g d s , |
|
7/12/2013 3:18 PM | |
Posts: 55 Rating: (1) |
Thanks for the reply SteBo SOrry I did not understood what you told me. I am not familiar with this scripting. Anyhow can u tell me the basics that what I am doing wrong and what should I put in that place. In FAQ two different picture windows are used and I want to use 1 for all Regards. |
Last edited by: Majeed Ahmed at: 7/12/2013 3:30 PMIn FAQ two different picture windows are used and I want to use 1 for all Last edited by: Majeed Ahmed at: 7/12/2013 3:30 PMIn FAQ two different picture windows are used and I want to use 1 for all |
|
Follow us on