7/11/2013 2:53 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hi random222a, Give us know the results |
7/11/2013 3:45 PM | |
Posts: 13 Rating:
|
I could not leave it On page 3-7 of attached pdf I found information, that only OP27 has hardware test, so it was normal that OP37 did not react for three arrows at startup. But on the same 3-7 page I found other three arrows for "Toggle between OP mode and DOS mode.". I used them. I thougth that, when I use them once, I'll get DOS mode, and when second time, I'll be back to autoloaded program. Nope. After first use, I got text on screen: "Drive not ready or disk boot failure. Insert or replace system disk then press <Enter> when ready." I turn off OP, pressed three arrows for toggle, and turned on OP, but it did not work. It still shows "Drive not ready...". I tried again and again, but still same text. How to get back to previous state? Please help me, or my guts will be split over the room... AttachmentOp2737_e.pdf (123 Downloads) |
7/11/2013 7:50 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello random222a Pl see Page 15-2 and 15-3 on procedure to enter Bios Setup and switch back to OP Mode. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
7/12/2013 8:53 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hi random222a, it is possible that the OP is the membrane keyboard that does not work, you solved the problem? |
7/25/2013 12:23 PM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating:
|
New question was splitted to OP37 backup in Prosave Best regards O_Moderator |
Follow us on