7/25/2013 9:09 PM | |
Posts: 3 Rating: (0) |
The machine is about 2 years old. CPU is 315-2AG10-0AB0, CP is brand new one ... 343-1CX10-... My Step7 V5.4, after catalog updates, always offers V2 for this CP - maybe this is a problem? I installed those modules several times before without problems. I tried solutions mentioned earlier in the thread to no avail. CP and CPU are in stop mode. Orange and red LEDS are on. I only have limited time to experiment - machine is in production 24/7 - so I did not try to remove other hardware and try CPU and CP only. see attached cfg file, cheers Attachmentsimatic 300(1).zip (235 Downloads) |
Follow us on