7/30/2013 1:36 PM | |
Joined: 9/23/2005 Last visit: 6/11/2024 Posts: 4346 Rating: (1433)
|
Hi, one of the innovations of the SP1 for STEP7 V12 (Released for Delivery at http://support.automation.siemens.com/WW/view/de/76276623)is related to rewiring of topological port connections. Now it is possible to change connections in topology view without the necessity to delete the previous connection. The attached cast shows how to operate it AttachmenttopologySP1.zip (260 Downloads) |
Last edited by: O_Moderator at: 7/31/2013 8:14 AMattachment reattached Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on