7/18/2007 9:29 PM | |
Posts: 95 Rating: (10) |
Howdy Yall’ I am sporting some bruises after getting bucked around the BSEND/BRCV!!! We need to put that one down it aint right! I am an ol’ LAD guy and brushed up against some of that indirect addressing stuff using STL – darn near finished my whole bottle of aspirin trying to make that work as a multiple instance in an FB. I left one of my boots in there and ran back to the safety of my PUT function. So for any brave engineering brother or sister who wants to take a stab at my PUT function I have placed the archive here and would love any feedback on why she aint right. Here is the skinny: I got her to work great AS LONG AS I do not start unplugging the cables or turning off the CPU’s (simulating real world faults). On the H-System if I am communicating to rack 1 for example and I turn off or unplug the cable in rack 0 the whole works goes down on rack 1 but I can still see rack 1 on accessible nodes. Go figure. I will try to nurse it along as best I can but any help would be greatly appreciated. But right now I need to go get another bottle of aspirin! Thanks Yall’ Darren (holding on till quitting time and a cold beer) in Dallas AttachmentPeer2peer_070718b_DK.zip (431 Downloads) |
Follow us on