9/9/2013 9:37 AM | |
Joined: 1/21/2013 Last visit: 6/2/2024 Posts: 4620 Rating: (705) |
Hi you've already seen this thread? Fault F0453 - Siemens Industry Online Support - Technical Forum ... |
9/9/2013 10:57 AM | |
Joined: 7/2/2010 Last visit: 1/22/2024 Posts: 50 Rating: (0) |
Yes i have already look at this thread but i do not think is my case because i do not any motor connected to the drive. |
9/11/2013 9:27 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
What is the control mode you using? I think for vector control (with or without sensor), you need to run motor. Try setting control mode to V/F scalor mode and try to run drive without motor. |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on