7/24/2007 9:46 PM | |
Posts: 2 Rating:
|
can anyone tell me if the S7-SCL programmig language can deal with files (like Pascal or C/C++) and if so, what kind of format has the file. thanks |
7/24/2007 11:27 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Seby, S7-SCL likes the most on Pascal, but is not the same. See the getting strted for some more information: S7-SCL V5.3 for S7-300/400 Getting Started or from the handbook: S7-SCL V5.3 for S7-300/400 |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/26/2007 2:46 PM | |
Joined: 8/10/2006 Last visit: 8/13/2024 Posts: 298 Rating:
|
If you've ever used the PSPad editor (great program! -- www.pspad.com -- freeware, but donate if you can!), here's a syntax file I use for highlighting SCL files. I find it very useful to edit a SCL source block offline and then import into the project Source.
AttachmentPCS7 SCL.zip (530 Downloads) |
Follow us on