(0)| 10/25/2013 1:53 PM | |
|
Joined: 1/28/2009 Last visit: 1/22/2026 Posts: 6892 Rating:
|
Hello, from products in range of SIMATIC,I can say "NONLIN" function from PID Professional package has the same functionality you want.But that package is used for S7 300/400 in TIA Portal.Same discussion we had before here.You have option of checking OSCAT library.But, for a programmer, that should not be really difficult to make such a function if points are limited.It is peicewise linear approximation of a arbitary function,define boundreis and in each boundry define the Y=AX+B formula. Hope these comments help Hamid Hosseini |
Follow us on