10/28/2013 6:58 AM | |
Joined: 3/10/2012 Last visit: 4/7/2022 Posts: 62 Rating: (0) |
Dear experts, I have a requirement like the attached file., in that file date and batch are buttons. there are 3 batches per day. when i select date and batch i need to get values like the sheet in hmi screen. Please help me. Waiting for your replay. Thanks and regards Sumesh
AttachmentData logging.pdf (67 Downloads) |
10/28/2013 7:48 AM | |
Posts: 112 Rating: (2) |
DEAR I THINK THIS WILL HELPS U FOR EXPORT AND IMPORT DATA FROM SQL SERVER AS DATA LOG How can you export data from the WinCC database into an ASCII file via a C script? What options do you have for exporting a database in SIMATIC WinCC? What options are there in WinCC for read and write access to TagLogging/AlarmLogging archives? |
10/28/2013 7:52 AM | |
Joined: 3/10/2012 Last visit: 4/7/2022 Posts: 62 Rating: (0) |
Dear sir, If possible, can you send me an example. Regards. Sumesh
|
10/28/2013 10:02 AM | |
Joined: 9/16/2011 Last visit: 9/10/2022 Posts: 291 Rating: (6) |
For that, You need have to create 50 real type address (=5 temp X 10 (from 8:00 AM to 12:30 PM)), that may be from some DB. And according to the time required, you may move the temp1, temp2, temp3, temp4, temp5 values to those addresses. Compiling these address into winCC you may show them on your HMI. see attachment to be cleared.
AttachmentATTACH.zip (55 Downloads) |
Reg, |
|
Follow us on