11/12/2013 12:37 PM | |
Posts: 4 Rating:
|
Dear All I am facing issue on VAV integration. The selected VAV controller & the VAV application is mentioned below. VAV Controller – RXC31.1 Actuator – GDB181.1E/3 Temperature Sensor – QAP22 No room unit is used.Selected application is-VAV04b The issue is even though the “DmpPosSu” shows 100% in the parameter list (SNVT) but in actual there is no voltage output available at analog output terminals. When we change the temperature set point w.r.t room temperature the “DmpPosSu” will vary from 0 to 100% accordingly but there is no voltage output available at analog output terminals. The same is observed in all the controllers . And further it is observed that when we select the VAV basic application ie “VAV01b” application we are getting the 0-10 VDC output at terminal YC1. But when we select the VAV application “VAV04b” for RXC31 no analog output available. The configuration settings for application VAV04b isattached here for your reference along with the system architecture Kindly provide the further solution for this AttachmentRXC31.1 configuration screen shots.zip (710 Downloads) |
Last edited by: Mahesha at: 11/18/2013 10:00 AM |
|
Follow us on