11/11/2013 9:23 PM | |
Posts: 4 Rating: (0) |
Hello, I would like to create visualisation of my process. I have CPU 314 IFM, PC and USB adapter. Communication by PC and CPU with MPI, visualisation - WinCC Runtime. But I have a small problem with Tags in WinCC, they are not visible. see attachment 1.jpeg When I give 24V on I124.0 input on CPU there is no change on visualisation. Connection parameters see attachment 2.jpeg Tag properties see attachment 3.jpeg In flexible version I have no problem with that, wincc flexible automatically created device which I join with cpu in netpro (step7) by mpi. Attachmentpictures.zip (68 Downloads) |
Last edited by: O_Moderator at: 11/12/2013 9:13 AMpictures transferred to attachment Last edited by: Damian77 at: 11/11/2013 9:25 PM |
|
11/12/2013 10:24 AM | |
Joined: 1/18/2008 Last visit: 3/20/2024 Posts: 36 Rating: (0) |
Hi What is the MPI System Parameters, Unit, Local Device Name set too? Cheers Andrew |
11/14/2013 10:49 AM | |
Joined: 1/18/2008 Last visit: 3/20/2024 Posts: 36 Rating: (0) |
I have a WinCC V7.2 application, running on a PC, connected to a CPU315 via a MPI USB cable. I have attached some of my configuration parameters, hope this helps. AttachmentMPI.zip (88 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on