7/24/2007 2:46 PM | |
Posts: 1275 Rating: (123)
|
Hi nikolas, Let's go through your message step-by-step... --> First, I've made an action in C Global Sricpt and save it as login_logut.pas. Then I have try to compile and it gave me back error that <ident> is expected before <eof> on the last line. Adding one } at the end of code solved the problem. Now, I have that script.... I copied the script without the initial and end statements, "{" and "}".... you probably placed it on top of one of them, so it was missing... --> Do I have to create that "LoginBit" and "LogoutBit" tags, and where? (in Internal tags?) --> Do I have to connect that script with those tags or with some other tag? -->In meantime I've figure it out part with tags and the connection with script. In the C-editor with opened login_logut.pas in Info/trigger I've set up triggering by @CurrentUser. Also ahve created LoginBit an LogoutBit in Internal Tags, and I've checked them with some symbols in Graphic editor. When I log in with some user the LoginBit is 1 (the LogoutBit is 0) and when I log out the LoginBit is 0 (the LogoutBit is 1). Is this ok? Have I do it right? I see you've already covered this... yes, they should be internal tags, as you've already noticed... You've already set the trigger properly as well... --> In Alarm logging I've already made a table with alarm messages, I dont want this messages about login/logut with them in the same table. Can I create a new table only with messages about login/logut? -->One more thing, maybe you didn't understand me exactly, I wanna to have a archive list of users logins, not only current messages if someone is loged in or if there is no one loged in. Is it possible with this script? In Alarm Logging you can configure different message classes... This allows you to filter, and display only the Login/Logout event messages, for instance... With this you can create reports with this type of message specifically... I've attached a .pdf with a step-by-step on how to create a class, a process value block and configure your message... Best regards, Danielle AttachmentUser.pdf (267 Downloads) |
7/25/2007 1:42 PM | |
Posts: 1275 Rating: (123)
|
Glad it helped! If you need anything else feel free to post! Best regards, Danielle |
Follow us on