11/27/2013 7:57 AM | |
Posts: 28 Rating:
|
Hello, I am using Simeas P P50,P55 V,I,KW,PF (4-20mA) hardwired Signals for Siemens PLC but When im connecting both AO from Siemeas P to PLC d value of analog is not stable continuously changing in Siemens HMI. When i read manual of siemeas P then i found these "The two channels of the module are not galvanically isolated against each other". Please anyone help me How can i use these analogs without adding any isolator??? Very Urgent!!!
AttachmentSIMEAS_P_en.pdf (353 Downloads) |
Last edited by: O_Moderator at: 11/27/2013 12:17 PMnew subject after splitting from /tf/WW/en/Posts/83562#top |
|
11/27/2013 12:18 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Regarding Simeas P (P50,P55) Hardwired Signal Exchange with S7-300. Best regards O_Moderator |
Follow us on