11/12/2013 10:20 AM | |
Posts: 17 Rating: (0) |
Hi, I am using two IO fields in picture window, which are linked through Structure tags. script run in Picture window. but if i change screen and change value in an IO field which has same tag, then it does not run. But if i switch to previous screen, that script run automatically. I know its pretty confusing what am writing so i have attached a few screen shots.They'll surely make it clear. AttachmentNew folder.zip (76 Downloads) |
11/26/2013 3:13 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40) |
Hi dark_alex, did you found a solution? If not, perhaps the technial support could help. Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
12/3/2013 10:58 AM | |
Posts: 17 Rating: (0) |
Hi, Lets say I want to change status of a bit. |
Follow us on