12/3/2013 9:08 AM | |
Posts: 1299 Rating:
|
Hello, what do you mean with "connect to wincc v12"? do you want to make a runtime for pc with which you have access to s7-1200? If yes, runtime professional or runtime advanced? Or do you want to make a project for a panel with wincc v12? Here are some examples for connection between hmi device and s7-1200 in V12: http://support.automation.siemens.com/WW/view/en/69864408 K!ke |
12/4/2013 9:23 AM | |
Posts: 1299 Rating:
|
Hello, you can access with 4 hmi devices to s7-1200 at the same time or 2 wincc systems. if you use runtime professional, you can only use single-station system. see these two chapters in manual for more information: WinCC Runtime Advanced WinCC Runtime Professional here you find information about s7-1200 with wincc flexible: http://support.automation.siemens.com/WW/view/en/38111886 K!ke |
Follow us on