11/25/2013 1:59 PM | |
Joined: 10/11/2006 Last visit: 5/23/2024 Posts: 5852 Rating: (793)
|
Hello, 6.5 Connection to the converter |
With best regards, |
|
12/6/2013 5:11 PM | |
Posts: 20 Rating: (0) |
Dear tech team thanks for giving this valuable info From below statement you reffered in attachment i have one more question which i would like you answer The standard insulation system is designed so that operation on the converter is possible for supply voltages up to 500 V +10% in motorized operation. Use a special insulation system or adopt special measures, e.g. output filter, for higher voltages. |
12/14/2013 6:00 AM | |
Posts: 20 Rating: (0) |
Dear experts awaiting your further comments |
12/16/2013 8:24 AM | |
Joined: 10/11/2006 Last visit: 5/23/2024 Posts: 5852 Rating: (793)
|
Hello, regarding the info: The standard insulation system is designed so that operation on the converter is possible for supply voltages up to 500 V +10% in motorized |
With best regards, |
|
Follow us on