1/29/2014 8:18 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
Hi, yes, it's possible. Have a look at this: Help of systemdiagnostics. Wüstenräuber |
This contribution was helpful to1 thankful Users |
1/29/2014 1:14 PM | |
Posts: 515 Rating: (56) |
hiWuestenraeuber, Thank you for the usefull link. Is it a seperate software package or only a tool?
|
1/29/2014 6:15 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello Wuestenraeuber Thanks for your reply. We don't have WinCC SCADA connected to the S7-300R ( SWR Redundancy ) . Instead it is connected to Vicos SCADA on IEC-104 protocol. Can we get the Diagnostic Status in the form of DB / Flag Bits in STEP7 so that we can map these to IEC addresses and transfer to VICOS ? Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on