12/26/2013 5:25 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Mike J Our Customer has All Relays ( SIPROTEC 4) on IEC-61850. I wants a Direct IEC61850 Connectivity ( Without Gateway / DC RTU ) to a local HMI besides a IEC-104 link with Remote SCADA. We had proposed a Redundant AK1703 Gateway in between the Relays and Local HMI / Remote SCADA. However the Customer wants that Local HMI should get data directly from the Relays. It is possible to use SICAM 230 as Local HMI directly communicating with the relays on IEC-61850 while simultaneously acquiring the data from Relays using a SICAM TM/AK1703 on IEC61850 and providing it to the Remore SCADA on IEC-104. Thanks for your advise in advance Navnag |
Last edited by: O_Moderator at: 12/29/2013 12:51 PMnew subject after splitting from /tf/WW/en/Posts/43784#top There is no such thing as the last bug in a program |
|
2/7/2014 5:30 PM | |
Posts: 340 Rating:
|
new question is splittet to gateway with storrage memory, AK1703 ACP has no storrage memory module. |
Follow us on