5/26/2014 7:53 AM | |
Joined: 6/8/2013 Last visit: 5/15/2024 Posts: 158 Rating: (9) |
hi, Which block is used for flow totalizer. i want to calculate total flow passing through line. Thanks
|
5/26/2014 8:00 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
First try this link: How can you accumulate physical flow measurements (e.g. mass flow rate, flow velocity) to an overall value? Then search Google as shown in attachment. Note: For Custody Transfer , in case of expensive material (liquid/gas) to transfer and exact volume is important ,specialized tools are used to calculate total flow with several additional signals(temperature/gas formation components ,...) to compensate the correct value.Search for "Flow Computer".
|
Last edited by: hdhosseini at: 5/26/2014 8:05 AMLast edited by: hdhosseini at: 5/26/2014 8:03 AM |
|
This contribution was helpful to2 thankful Users |
5/29/2014 11:46 AM | |
Posts: 73 Rating: (6) |
Hi, You could create a simple totalizer block to calculate the accumulated flow. Here is one sample totalizer / intergrator block which you could make use of. Regards, Krrish !! AttachmentC:\Dump\Dump\HDD Backup\E\Miscellaneous\Sources\Totalizer.zip (642 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on