11/1/2011 8:25 AM | |
Posts: 5 Rating: (0) |
I want towrite the position of a NC axis into the PLC for an additional position readout. Anybody got an idea? |
11/1/2011 9:19 AM | |
Joined: 1/29/2008 Last visit: 7/26/2022 Posts: 419 Rating: (19) |
Hi You can use NC Var Selector. Good luck Nit |
11/2/2011 5:55 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Hi, As nit said you can use NC VAR to read the Axis position in PLC. Find the attached steps of NCVAR & Example plc to read the Axis value. AttachmentNCVAR.zip (686 Downloads) |
Regards, |
|
This contribution was helpful to1 thankful Users |
1/17/2013 6:26 AM | |
Joined: 4/8/2010 Last visit: 7/26/2022 Posts: 3 Rating: (0) |
Thanks a lot... |
6/16/2014 4:39 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoCommunication between PLC & HMI went off & PLC gone to stop modeand closed. Please use the original topic for discussion:WIn Ac MP 377 communication With best regards, Narrator1
|
Follow us on