(0)| 6/20/2014 7:49 AM | |
|
Posts: 17 Rating:
|
Hi, Please check with directly shorting the enable signals i.e terminal 9, 112 & 48, terminal NS1 & NS2, ternal 63 & 9, terminal 64 & 9.... in this situation the drive shoud go to ready mode i.e only you shoud get orange (yellow) led in ON condition.... if it is working ok then you need check the wiring for further diagnosis. Please refer the attached 611A Startup manual from page no - 26 onwords. Hope it may help you. As looking to the MLFB no of the module is older version (out dated) the comonents may be weaken. Regards, Santosh Attachment611A Manual.pdf (952 Downloads) |
| 6/20/2014 4:17 PM | |
|
Posts: 18 Rating:
|
Hi Santosh, Thank you very much for the advice and link to the manual, will continue troublshooting, have a great day! |
Follow us on